STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC accuracy without internal re-calibration

Hello,I have an application, where I need ADC samples at a fixed rate, if the device is running. So, I can do a ADC self-calibration at start up and while idle, but not while the application is running.The application can run for several hours and th...

T B by Associate II
  • 854 Views
  • 0 replies
  • 0 kudos

Resolved! SPI using DMA on STM32F103 transmits one word too much

On an STM32F103 I configure SPI in 16bit wide mode and set up a DMA transfer to transmit one word:SPI2->CR1 &= ~SPI_CR1_SPE; SPI2->CR2 = 0; SPI2->CR1 = SPI_CR1_SSM | SPI_CR1_SSI | SPI_CR1_DFF | SPI_CR1_SPE | /* Some baud rate flag...

How do I read the RTC on the STM32L433 after power up.

Hi I am using the RTC on the STM32L433 with battery backup. After the date/time been set and running , then either processor reset or repoert the unit the date/time resets to the default time. As it happens even after reset (power not disconnected) ...

How to turn on backup RTC registers on STM32F051R8T6

Hello, i have probem with backup registers, which are powered from VBAT pin on Dicsovery board.First problem was CubeMX init, where i can't choose LSE source, because the value of clock box, was not active. I tried differend things like change txt c...

shybiss by Associate
  • 916 Views
  • 0 replies
  • 0 kudos

Which pins are needed to program a mcu via swd

hello everyone !i'm using a nucleo board (NUCLEO-F401RE) to program a MCU STM32F301 placed on newly fabricated pcb; the mcu has never been programmed.i have disconnected the jumpers to use the CN4 connector. i have just connected the SWCLK (clock sig...

ABoya.14 by Associate II
  • 20317 Views
  • 8 replies
  • 0 kudos

Can we continuously read registers using I2c ?

i have interfaced opt8320 optical sensor to stm32f446zet.I hav configured STM as master and Opt8320 as Slave. Can i initiate continuous registers read from sensor using I2c ?Please share suggestions regarding this issue.

Amal Babu by Associate III
  • 1347 Views
  • 4 replies
  • 1 kudos

Resolved! Oscillator calculation STM32

I want to use a STM32F103, STM32L431, 451 and 471 microcontroller, but i don´t know if the crystal that i selected (ABS07-120-32.768kHz-T and ABMM2-8.000MHZ-E2-T) is valid for this microcontroller.And another question is how to calcule the load capac...

Problem with the RCC LSE STM32L496RET6 MCU.

Hello! I use CubeMX to generate the init code for rcc whith LSE Crystal NX3215SA-32.768KHZ-EXS00A-MU00525 (32.768K,6PF), two 2.7pF capacitors and rtc module. Program goes to error handler after "if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)"-s...

RAkma by Associate II
  • 3076 Views
  • 6 replies
  • 0 kudos

How to drive the emmc chip in stm32l4r5 ?

hello. I am an embedded software engineer from China ,At the moment I'm tryingDrive emmc on stm32l4r5 ,but I failed .Who can give me a demo about how to drive emmc on stm32l4xx , thank you​

ydong by Associate II
  • 2053 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.