2014-01-20 11:32 AM
2014-01-21 2:38 AM
Hi
''but problem is that program works fine, before os_evt_wait_or() just when program arrives to line 69(exactly where the task is in the wait_or() ), it stops!!!'' That is because the IRQ for the timer is not triggering and NOT sending the task message. Check the timer setup is correct. The timers are tricky to use if you use anything other than the basic up/down counter/reset count. You are going to have to read and re-read the reference manual - the timer section! '' /* Clear TIM4 Capture compare interrupt pending bit */ TIM_ClearITPendingBit(TIM4, TIM_IT_CC2); /* Get the Input Capture value */ IC2Value = TIM_GetCapture2(TIM4);'' You should do the above code in the ISR - NOT the task body.2014-01-24 9:07 AM
man, thanks
it solved.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.