2014-01-24 8:56 AM
Hello,
I try to write a simple LED blink with delay by SisTick. But, IAR EWARM keep giving me error, ''SysTick_IRQn'' has already been declared in the current scope'', with SysTick ISR. So I clicked the error message. It leaded me to the line below in stm32f4xx.h. SysTick_IRQn = -1, /*!< 15 Cortex-M4 System Tick Interrupt I tested a similar code with Keil. Keil didn't give the error. Please let me know any mistakes. Thanks.&sharpinclude <stm32f4xx.h>
&sharpinclude <stdio.h> &sharpinclude <stm32f4xx_rcc.h> &sharpinclude <stm32f4xx_gpio.h>void GPIO_Configuration(void)
{ GPIO_InitTypeDef GPIO_InitStruct; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_12|GPIO_Pin_13|GPIO_Pin_14|GPIO_Pin_15; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOD, &GPIO_InitStruct); }volatile unsigned int msTicks;
void SysTick_IRQn(void)
{ msTicks++; }void Delay (unsigned int dlyTicks)
{ unsigned int curTicks;curTicks = msTicks;
while ((msTicks - curTicks) < dlyTicks); }void main(void)
{ GPIO_Configuration(); /* max para should be 2^24-1 = 16777215 = 0xFFFFFF, Systic clock = HCLK = 168MHz. */ /* ms tick. */ SysTick_Config(SystemCoreClock / 1000); while(1) { GPIO_SetBits(GPIOD, GPIO_Pin_12); // LED4, Green on GPIO_ResetBits(GPIOD, GPIO_Pin_13); GPIO_ResetBits(GPIOD, GPIO_Pin_14); GPIO_ResetBits(GPIOD, GPIO_Pin_15); Delay(50);GPIO_ResetBits(GPIOD, GPIO_Pin_12); GPIO_SetBits(GPIOD, GPIO_Pin_13); // LED5, Orange on GPIO_ResetBits(GPIOD, GPIO_Pin_14); GPIO_ResetBits(GPIOD, GPIO_Pin_15); Delay(50); GPIO_ResetBits(GPIOD, GPIO_Pin_12); GPIO_SetBits(GPIOD, GPIO_Pin_14); // LED5, red on GPIO_ResetBits(GPIOD, GPIO_Pin_13); GPIO_ResetBits(GPIOD, GPIO_Pin_15); Delay(50); GPIO_ResetBits(GPIOD, GPIO_Pin_12); GPIO_SetBits(GPIOD, GPIO_Pin_15); // LED5, red on GPIO_ResetBits(GPIOD, GPIO_Pin_14); GPIO_ResetBits(GPIOD, GPIO_Pin_13); Delay(50); }
} #stm32f4-discovery-sistick
2014-01-24 9:36 AM
void SysTick_IRQn(void)
{ msTicks++; } No this should be SysTick_Handler(void) it's a function, not an index into the NVIC/SystemHandler table.2014-01-24 9:41 AM
Hi
There must be another define somewhere. Or the file stm32f4xx.h has been included twice in a file somewhere. Another possibility is the file stm32f4xx.h has been added twice in the IAR project settings.2014-01-24 10:28 AM
Thank you so much!
I confused SysTick_Handler with SysTick_IRQn. I used SysTick_Handler in Keil that's why I didn't get error. Problem was solved. Thanks again.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.