2020-07-20 1:51 AM
Hello,
I am writing a project with STM32H7. The project contains RTC, SPI, USART, SD Card, timers, and I2C.
In order to have more RAM, I have brough the data and bss to RAM_D1.
As next steps I want to implement Ethernet. However, I realized that in order for Ethernet to work, I need to only use RAM_D1.
The problem is when I bring the heap and stack to RAM_D1, the project stops working.
Can someone please help?
I include the linker script before and after bringing everything to RAM_D1.
Thank you in advance for your help.
Solved! Go to Solution.
2020-07-20 8:00 AM
I am using the single core (STM32H753). Right now I have put the .bss and the .data on the RAM_D1 and the heap and stack on DTCMRAM and it is working fine. However, for implementing Ethernet I need to bring also the heap and stack (as i have read and so far understood) to RAM_D1, and when I do so peripherals stop working (SPI and USART as far as it is visible to me).
2020-07-20 8:04 AM
Thank you for your reply, I did it but again everything stopped working.
2020-07-20 11:27 PM
it is a single core (STM32H753), and I am currently using RAM_D1 for .bss and .data, and DTCMRAM for heap and stack, and until here everything works. However for implementing Etherner I need to bring the heap and stack into RAM_D1, and when I do so the whole system stops working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.