STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC external trigger input

Hi I'm developing an application which I tested on the nucleo board and I want to make my custom board. I went through the datasheet of STM32Go71kb(32 pin version) and I could not find the ADC external trigger input pin. Additonally I cannot provide ...

BDasa.1 by Associate II
  • 1634 Views
  • 0 replies
  • 0 kudos

Resolved! problem when changing from DTCM Ram to RAM_D1

Hello, I am writing a project with STM32H7. The project contains RTC, SPI, USART, SD Card, timers, and I2C. In order to have more RAM, I have brough the data and bss to RAM_D1. As next steps I want to implement Ethernet. However, I realized that in o...

VYoun by Associate III
  • 8995 Views
  • 12 replies
  • 0 kudos

STM32L011F3 ADC Calibration

Hi Sir,In STM32L0 ADC, there is a feature call ADC calibration.I would like to know, after performing ADC calibration, do I have to do factoring using the CALFACT (calibration factor obtained after running ADC calibration) in the result I obtained fr...

How to generate Center Aligned PWM with variable duty cycle that has PWM frequency of 1.5MHz with dead time insertion?

Hello,I need to be able to generate a center aligned PWM signal on two Ch. with 1.5MHz PWM frequency. The duty cycle variation will have dead time inserted in it. In order to generate 1.5MHz for center aligned signals, I need to calculate ARR Registe...

MS.1134 by Associate III
  • 4643 Views
  • 7 replies
  • 0 kudos

STPM4Raspi

Hello,I'm using STPM4Raspi (ST33TPHF2ESPI) on Linux.For performance reasons, I would like to use the Linux driver (tpm_tis_core.c) in interrupt mode. Hence I've added the support in the Linux device Tree. The linux driver tries to probe the interrupt...

Kurt by Associate
  • 763 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.