2025-04-20 11:21 AM
Hey,
I have a STM32H743IIT Board with an QSPI W25Q128J Flash, i use LTDC and LVGL.
I want to store my pictures in the Flash Memory, but i have some Problems with the External Loader or the Mapping, or something.
The Flash workes fine, when i Write a buffer and Read a Buffer from the Program itself.
I'am a little confused, in the reference guide from the STM32H743IIT, is the Bank 1 located at 0x60000000, but in some examples, are the address 0x90000000 used.
I tried with the CubeProgrammer and the Loader "M29W128GL_STM32H743I-EVAL", here is the Pagesize 0x10, and Startaddress 0x60000000, with these can i erase the complete external memory without errors, but the Pagesize of the W25Q128J is 0x100 (256) ....
Download from STMCubeIDE don't work, i get the Error:
[224.387] spawnCubeProgrammer(): 19:46:26:421 w ap 0 @0x24033710 : 0x0002D690 bytes, Data 0xFFFFFFFF...
[224.387] spawnCubeProgrammer(): 19:46:26:421 W B2 in RAM @0x24042E80 size 0x0002D690: 1247ms
[224.387] spawnCubeProgrammer(): 19:46:56:000 Wait W B1 in Flash @0x60000000 size 0x0002D690: 29579ms
[224.387] spawnCubeProgrammer(): 19:47:56:000 Write elapsed time: 91993ms
[224.387] spawnCubeProgrammer(): 19:47:56:000
[224.387] spawnCubeProgrammer():
[224.387] spawnCubeProgrammer(): 19:47:56:000 Error: failed to download Sector[0]
[224.387] spawnCubeProgrammer(): 19:47:56:000 Error: failed to download the Filemy .FLASH:
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
QSPI (r) : ORIGIN = 0x60000000, LENGTH = 16M
AREA1 (rx) : ORIGIN = 0x081E0000, LENGTH = 128K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
my test file to upload is ca 32 kb...:
const __attribute__((section(".extFlash"))) uint8_t img_logo_map[] = {
0x1a,0x17,0x15,0xff,0x1a,0x17,0x15,0xff,0x1a,0x17,0x15,0xff,0x1a,0x17,0x15,0xff,0x1a,0x17 .......};Is there a W25Q128J Loader for the STM32H743 with QSPI ?
2025-04-20 6:11 PM
>>I'am a little confused, in the reference guide from the STM32H743IIT, is the Bank 1 located at 0x60000000, but in some examples, are the address 0x90000000 used.
Yeah, 0x60000000 is FMC Bank 1 for Parallel NOR Flash, the QSPI NOR FLASH will be at 0x90000000. Perhaps you can show the RM page/diagram you're talking about..
>>Is there a W25Q128J Loader for the STM32H743 with QSPI ?
Got all sorts of parts and pin configurations
https://github.com/cturvey/stm32extldr/tree/main/h7_w25q128
2025-04-21 1:13 AM
> Yeah, 0x60000000 is FMC Bank 1 for Parallel NOR Flash, the QSPI NOR FLASH will be at 0x90000000. Perhaps you can show the RM page/diagram you're talking about..
ah okay, i looked in the fmc table, but i am blind to find the right page?
> Got all sorts of parts and pin configurations
No, my configuration (PB2, PB10, PF6, PF7, PF8, PF9) is not available..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.