STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f429i-disc sdram fb with ltdc

Hy,  i am new here and need help. Is there an exemple of a cube ide project with all the important files like .ioc ect.?I have problems with the onboard display.I use the sdram bank2 as framebuffer (startaddress 0xd0000000). I can see (mem window) th...

Interfacing the LTC1403 SPI ADC

Hi there,I'm currently trying to get SPI Communication with the LTC1403 up and running, however I'm struggling with the timing of the Conv Signal.It seems like I need the rising edge of SCK at the same time as the Conv Signal is high. How can I achie...

always_energized_0-1745156290531.png

Resolved! Synchronous start of three timers

Hello everyone. Question about synchronous launch of three timers.Given:- CPU F0 or F4 or G4 (of course F103 is possible - I just don't like it, personal dislike);- three timers, each with its own operating frequency, Timers work via DMA, each with i...

Aflik by Associate II
  • 1191 Views
  • 2 replies
  • 0 kudos

Problem with programming

Hello everyone,I am kind of new to STM chips, i have a problem regarding programming the chip. I don't use any board, only chip on the SMD to DIP board. But when i want to program it using st-link, STM32cube can identify the programmer but not the ch...

Mohade by Associate
  • 1225 Views
  • 3 replies
  • 2 kudos

Resolved! Use of bootloader to program an STM32G474QET6TR

Hello, I am designing a card that will use an STM32G474QET6TR and I want to program it using USART. The card will use a USB to USART converter (FTDI4232HL).  The Rx and Tx of the FTDI are connected to pin PA2 and PA3 respectively, as I found in AN260...

EliazLB_0-1744113604627.png
EliazLB by Associate III
  • 2122 Views
  • 4 replies
  • 1 kudos

Resolved! STM32N6 minimal hardware design

Hi there,I'm designing a custom PCB using the STM32N657Z0 MCU. The design is extremely space-constrained, so I try to leave out everything I can. Since this deviates quite a bit from the reference design (well, the N6 Discovery kit, that is) I'd love...

asdfasdf by Associate III
  • 3993 Views
  • 5 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.