2018-04-15 2:27 PM
I am following the example code found here to send and receive CAN messages:
STM32Cube_FW_F4_V1.21.0\Projects\STM324xG_EVAL\Examples\CAN\CAN_Networking\Src
I can happily receive CAN messages but when I call the following code, the CAN message is never sent.
HAL_CAN_AddTxMessage( &hcan1, &TxHeader, TxData, &TxMailbox );
while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan1) != 3) {}TxHeader is configured as:
TxHeader.StdId = 0x123;
TxHeader.ExtId = 0x01; TxHeader.RTR = CAN_RTR_DATA; TxHeader.IDE = CAN_ID_STD; TxHeader.DLC = 7; TxHeader.TransmitGlobalTime = DISABLE;And TxData is filled with seven bytes of data.
HAL_CAN_GetTxMailboxesFreeLevel always returns 2 and I don't see the CAN message on the bus.
Any help or idea would be gratefully appreciated.
Andy
2018-04-16 4:57 AM
:
2019-01-27 3:18 PM
Hi,
I have same problem about 2 weeks i stuck in here, please can you explain how could you solve this problem?
Thank you, best regards.
2019-01-27 4:26 PM
2019-01-28 12:19 AM
Thank you so much TJ i tried again in debug mode TxMailbox is always equals to 0x00000001 and the txdatas are not written in TxMailbox even if the selected mailbox(0) is empty why behave like this
Best regards.
2019-01-28 12:24 AM
WRITE_REG(hcan->Instance->sTxMailBox[transmitmailbox].TDHR,
((uint32_t)aData[7] << CAN_TDH0R_DATA7_Pos) |
((uint32_t)aData[6] << CAN_TDH0R_DATA6_Pos) |
((uint32_t)aData[5] << CAN_TDH0R_DATA5_Pos) |
((uint32_t)aData[4] << CAN_TDH0R_DATA4_Pos));
WRITE_REG(hcan->Instance->sTxMailBox[transmitmailbox].TDLR,
((uint32_t)aData[3] << CAN_TDL0R_DATA3_Pos) |
((uint32_t)aData[2] << CAN_TDL0R_DATA2_Pos) |
((uint32_t)aData[1] << CAN_TDL0R_DATA1_Pos) |
((uint32_t)aData[0] << CAN_TDL0R_DATA0_Pos));
I think there is a problem but i dont know thanks for help.
2019-01-28 10:18 PM
2019-01-28 11:53 PM
2019-01-29 12:01 AM
thank you for your interest...
I have datas like these;
TxData[0]=0x11;
TxData[1]=0x12;
TxData[2]=0x13;
...
2019-01-29 12:29 PM
2019-01-29 12:37 PM
CAN_TDH0R_DATA7_Pos=0x00000018
CAN_TDH0R_DATA6_Pos=0x00000010
CAN_TDH0R_DATA5_Pos=0x00000008
CAN_TDH0R_DATA4_Pos=0x00000000
CAN_TDL0R_DATA3_Pos=0x00000018
CAN_TDL0R_DATA2_Pos=0x00000010
CAN_TDL0R_DATA1_Pos=0x00000008
CAN_TDL0R_DATA0_Pos=0x00000000
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.