2017-07-13 9:28 AM
Hi,
I have an STM32 and am trying to receive a single byte of data from a CC2540 over UART. I've verified that the data transmission from the CC2540 is working properly (I can receive the data in a serial terminal) but for some reason the data is not being received by the STM32. I am using USART3_IRQ on the STM32 and have verified that it is working properly (I can trigger USART3_IRQ by sending test data from a serial terminal).
Can anyone help me with this? It's very puzzling.
Cheers,
Tony
#uart #stm32 #cc25402017-07-13 10:01 AM
>>
Can anyone help me with this? It's very puzzling.
Even more so with no HW or SW to look at.
2017-07-17 9:04 AM
I am using a custom pcb with an onboard STM32 and CC2540 physically connected together over USART3. I have programmed the CC2540 to relay a single byte of data over USART3 and programmed the STM32 to receive this data in USART3_IRQ. Here is the relevant code from each device:
1) CC2540 (BLE_Bridge):
static void simpleProfileChangeCB( uint8 paramID )
{ uint8 data[20]; uint8 len; switch( paramID ) { case HORIZON_VALUE: SimpleProfile_GetParameter( HORIZON_VALUE, &data ); len = data[0]; //keep trying to send data until it is a success. this may not be the desirable approach while (sendDataToHost(&data[1], len)); break;default:
// do nothing break;}
}2) STM32:
void USART3_IRQHandler(void)
{ RXNE_flag = USART_GetFlagStatus(USART3, USART_IT_RXNE); RXNE_IT_status = USART_GetITStatus(USART3, USART_IT_RXNE); if(RXNE_IT_status != RESET){ horizon_val = (s16) USART_ReceiveData(USART3); }}As I said, I can successfully send data to the STM32 through a serial terminal so USART3_IRQ should be triggered when the CC2540 transmits the data.
I have configured USART3 on the CC2540 to use DMA, do I have to use DMA on the STM32 as well?
Tony
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.