2019-08-01 11:16 PM
I am writing an app to evaluate the STM32L433. I am using the RTC peripheral, setting an Alarm, and processing an interrupt on it.
During my development, I wanted to disable interrupts momentarily using the debugger. For this, I tried to modify PRIMASK but I realised it is always reading back 0x0.
I found that if I use the debugger to set PRIMASK to 0x1, then interrupts are disabled and my Alarm does not trigger. When I used the debugger to set it back to 0x0, I expected my interrupt to trigger since the correct flag is set in the ICPR1 register but this did not happen.
Should I be able to manipulate PRIMASK using the debugger? If I should, then why did my interrupt not trigger after changing PRIMASK back to 0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.