STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F429 video output protocol for a SVGA display

Hello,I'm looking to use the STM32F429 to output data to an SVGA display. The supported video formats for the display are shown in the image below. The display is actually a monochrome variant, so color is not relevant as the RGB lines are tied tog...

0690X000009ZhkeQAC.jpg
MRyan.7 by Associate III
  • 1345 Views
  • 1 replies
  • 0 kudos

QSPI error at border 0x01000000

Chip stm32f746, memory S25FL256S in 32-bit address mode.An error occurred while sharing DMA and reading directly on the edge of the address 0x01000000.The error occurs when the high fourth byte of the memory address is changed. When DMA and reading o...

SDRAM and adc warnings

I am evaluating the STM32F767NIH. I am finding the warnings a bit unclear for the FMC. A brand new project with only the fmc shows a warning triangle that I can't seem to get rid of. I have checked Clock and chip enable SDCKE0+SDNE0, 2 banks, 13 bi...

_EFrie by Senior
  • 877 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H7 - USB HS Host - nothing happens

Hi there,​I got some troubles getting the USB Host system working on the STM32H746ZI.​Worth mentioning is that this is no dev board here, just a plain H7 mcu on a DIY bread board. It is properly supplied with filtered 3.3 and 1.8V. Got UART, I2C, LCD...

Microman by Associate III
  • 8240 Views
  • 10 replies
  • 1 kudos

what's the problem?

hello everyone,can someone help me please, I can't understand why I can't receive 7, it's weird... I sent 7 , i want to receive 7, but I receive 255, 0, 15.. all the values except 7, that's really insane.

0690X000009ZeWtQAK.png
idrissmc by Associate III
  • 6583 Views
  • 20 replies
  • 0 kudos

CAN_ESR LEC[2:0] Error meanings

These are the CAN error codes listed in RM0008 (Manual for STM32F1)Is there anywhere in documentation that says what they actually mean in detail? Are these detected on RX or TX. I assume that in this case its TX and, while active an error frame will...

DJC by Senior
  • 2609 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.