2017-07-05 5:32 AM
Have been playing with the B-L072Z-LRWAN1 and it all works fine. Now we would like to hook up directly to the Murata ABZ (via the break out / CN2 and CN3).
As a start I have externally powered the ABZ. I expected the ABZ to send out LoRa messages as it does when connecting the Disco board via USB. However there are no LoRa message getting out. What am I missing here? Suggestions are appreciated
Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-01-08 10:07 AM
Hello Jeroen,
I'm also trying to get USART1 working instead of LPUART, I did following changes besides the one related to the GPIO that you already posted but no luck. Could you please provide some hints?
&sharpdefine UARTX USART1
&sharpdefine UARTX_CLK_ENABLE() LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1)&sharpdefine UARTX_RX_GPIO_CLK_ENABLE() LL_IOP_GRP1_EnableClock(RCC_IOPENR_GPIOBEN)&sharpdefine UARTX_TX_GPIO_CLK_ENABLE() LL_IOP_GRP1_EnableClock(RCC_IOPENR_GPIOBEN)&sharpdefine UARTX_FORCE_RESET() LL_APB2_GRP1_ForceReset(LL_APB2_GRP1_PERIPH_USART1)
&sharpdefine UARTX_RELEASE_RESET() LL_APB2_GRP1_ReleaseReset(LL_APB2_GRP1_PERIPH_USART1)&sharpdefine UARTX_IRQn USART1_IRQn
&sharpdefine UARTX_IRQHandler USART1_IRQHandler2018-01-08 11:15 AM
If the pins are PA9/PA10 then you'd need to enable GPIOA clocks, not GPIOB clocks
Use a debugger and walk the pin and peripheral settings.
Do some sanity checking by sending a byte stream (0x55 ?), scope pins, confirm bit timing and signal presence.
Check the interrupt handler fires.
&sharpdefine UARTX USART1
&sharpdefine UARTX_CLK_ENABLE() LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1)&sharpdefine UARTX_RX_GPIO_CLK_ENABLE() LL_IOP_GRP1_EnableClock(RCC_IOPENR_GPIOAEN)&sharpdefine UARTX_TX_GPIO_CLK_ENABLE() LL_IOP_GRP1_EnableClock(RCC_IOPENR_GPIOAEN)&sharpdefine UARTX_FORCE_RESET() LL_APB2_GRP1_ForceReset(LL_APB2_GRP1_PERIPH_USART1)
&sharpdefine UARTX_RELEASE_RESET() LL_APB2_GRP1_ReleaseReset(LL_APB2_GRP1_PERIPH_USART1)&sharpdefine UARTX_TX_PIN GPIO_PIN_9
&sharpdefine UARTX_TX_GPIO_PORT GPIOA&sharpdefine UARTX_TX_AF GPIO_AF4_USART1&sharpdefine UARTX_RX_PIN GPIO_PIN_10&sharpdefine UARTX_RX_GPIO_PORT GPIOA&sharpdefine UARTX_RX_AF GPIO_AF4_USART1&sharpdefine UARTX_IRQn USART1_IRQn
&sharpdefine UARTX_IRQHandler USART1_IRQHandler2018-01-09 2:25 AM
You will also have to make sure that the go-to-sleep and wake-from-sleep stuff is properly handling your changes ...
Have you looked at theI-NUCLEO-LRWAN1
- with the
USI module? This seems more focussed on being just a 'modem' (with AT Commands) - rather than having embedded applications?http://www.st.com/en/evaluation-tools/i-nucleo-lrwan1.html
It has a smaller STM32, so might work out cheaper when not needing all the extra flash ... ?
2018-01-09 7:01 AM
Thanks Clive,
Yeah with your code so far I'm able to observe PA9 on the scope after system reset.
It seems that I need to adjust a clock somewhere because the baudrate decreased from 9600 to 9
I'm working with STM32 for the first time, any help is appreciated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.