STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Minimum HCLK value for STM32F7?

Posted on January 09, 2018 at 13:50 I am working on STM32F777 where I see that cubeMX does not allows me to enter HCLK value below 16MHz. 1.) Is there a way to make it lower to something like 2 or 4MHz? 2.) How should I select clock frequencies...

STM32L071 comperator vrefint bug in HAL and Ref Manual

Posted on January 09, 2017 at 11:41Hi,I have found a bug for STM32L071xx series in using the comperators with vrefint in the actual Reference Manual V7.0 and the actual HAL STMCubeL0 V.1.7.0:When selecting the the vrefint for the comperator minus in...

Power Profiling Tool for STM32 Applications

Posted on August 02, 2016 at 06:52In the STM32CubeMX there is Power Consumption Calculator Tool.But this is for new code to be developed.Is there any other tool or this tool available for the already developed Application?There is tool for TI's MSPs...

darla14 by Senior
  • 2353 Views
  • 2 replies
  • 0 kudos

hi,i am using 32-bit compiler in my ubuntu14.04 lts.i got my compiled with arm-none-eabi.but when i migrate it to 64-bit linux machine, code size increased and there were errors insuffient .data section.how can i resolve this ? , hi,i am using 32-bit comp

Posted on January 09, 2018 at 16:12i am using 32-bit linux(local machine).my source code compiled and bin file generated properly.but when i compiled the same sources on 64-bit machine(server),.data section is excedded the limit of stm32 controller....

Power LoRa disco board external

Posted on July 05, 2017 at 14:32 Have been playing with the B-L072Z-LRWAN1 and it all works fine. Now we would like to hook up directly to the Murata ABZ (via the break out / CN2 and CN3). As a start I have externally powered the ABZ. I expected ...

Resolved! STM32F105 flash erase problem

Posted on June 16, 2017 at 16:56Hello!Got a weird problem with STM32F105R8T6 chipWhile the same code, compiled and running on  STM32F103R8T6, works okProgram size is 17 kB as can be seen from map file:AHBPrescTable 0x0800473a Data 16 system_stm32f1x...

yury by Associate II
  • 2761 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.