2010-05-21 8:55 AM
Pong game or composite video for STM32
#cortex2011-05-17 4:52 AM
LCD screens are ok but what if someone wants composite video to create a game console? I am looking for the exact same thing. so if someone knows a open source code for a PONG game on a oposite video i would be more than happy.
Thanks R2011-05-17 4:52 AM
Here 30 years in the future, we use LCD screens.
2014-04-18 7:55 PM
This may not be helpful, but I thought i would just post it, since it was a solution that worked for me.
https://sites.google.com/site/suprabotics/stm429-discovery-expansion-board-v2-0/home After trying with no success to get the timing right for the STM32F429I-Discovery board to generate a composite video output (to display on a small TV set), I just gave up on the whole TV composite conceptI wired the H-Sync, V-Sync, RGB input pins of an old Samsung VGA monitor directly to the pins on the discovery board (only used B7, C7, and G7 pins for a total of 8 colors, similar to the arcade machines of old.)I translated the code for the VGA_Demo from Keil to em::blocks. Easy! Results: A 640x480 color screen with 8 colors. Cost equals Zero!Graphic library is included in the code. Draws, fills, geometry, buffering, screen copy, sprites, etc.Code up your own Pong Game ;)Beats trying to run on a tiny 2.5 inch LCD Screen.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.