STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DCMI STM32F40x CAMERA VSYNC ISSUE

Posted on April 15, 2014 at 15:06Dear All,I'm initialising the DCMI and DMAing camera data fine. The problem comes when I reset and then re-initialise the DCMI after disabling and then re-enabling the camera. The DCMI doesn't seem to wait for the fi...

kirem by Associate II
  • 2287 Views
  • 3 replies
  • 0 kudos

STM32F4 APB1 Prescaling Issue

Posted on April 19, 2014 at 10:54Hi all, I'm curious about prescaling APB1 for the STM32F4. I'm building a triangle wave generator and frequency meter, for which it is conveniant for me to have a high as possible clock frequency for Timers 4 and 6....

jono-tree by Associate II
  • 1493 Views
  • 1 replies
  • 0 kudos

Transfer data form STM32 to Linux

Posted on December 10, 2013 at 03:19Hello everyone, I wrote a hello world program, which is used eCos, for STM32F4 Cortex-M4 platform. Then, I type the command, which is sudo screen /dev/ttyUSB0 -115200, to see the result in the Ubuntu 12.04. It alw...

gapryun by Associate II
  • 1942 Views
  • 4 replies
  • 0 kudos

USB D+/D- voltage versus STM32F103 VDD voltage

Posted on April 18, 2014 at 19:24Hi,You probably already get such discussion.I am currently designing a board based on STM32F103RC6 MCU that I want to supply with Vbat=3V6, VDD1/VDD2/VDD3/VDD4=VDDA= 2V4 but in the data sheet, the Vdd min in the USB ...

bertrand by Associate
  • 1135 Views
  • 0 replies
  • 0 kudos

ITM_ReceiveChar (void) gives undefined.

Posted on January 11, 2012 at 21:46Using ITM_ReceiveChar (void) I get the error  ''undefined reference to `ITM_RxBuffer'''.  I am able to successfully use ITM_SendChar() as evidenced by getting the corresponding output on my SWV Console so my proble...

jdsotack by Associate II
  • 3778 Views
  • 4 replies
  • 1 kudos

Crystal drive level

Posted on September 22, 2011 at 11:31I have read the ST app note about crystal oscillators and I am concerned about the drive level. Before reading this app note, I chose the TXC 7M series crystals for its small size and reasonable cost. In the data...

Can't set character match bits in USART_CR2

Posted on April 18, 2014 at 02:58I'm trying to generate a reset on a USART receive character match on the F3 Discovery board. If I understand the user manual, I need to set bits 31:24 of USART_CR2 to be the character I want to match. The problem is ...

Linking errors when redirecting stdout to uart on stm32f2

Posted on April 17, 2014 at 22:50Greetings,I'm working with an stm32f215rg mcu and I'm attempting to redirect stdout/in to uart4. I seem to be getting linking errors when attempting to link all the objects/libs together. The line I use is below:arm-...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.