2016-07-11 7:08 AM
Hi,
I want to write a phase comparator on my nucleo-f334.As far as I know, it works like this: two signals are sent in the phase detector. When one of them cross the zero line, a timer/counter is started, and it stops when the second signal cross the zero line. The phase detector outputs the difference between the two phases from the value of the counter.I think it is supposed to raise a flag or provoke an event when the first cross the line to start the count, and another one to stop it. But lacking of knowledge in this domain I don't know how to do it, and the results I find on the internet are almost exclusively about simulating a PLL, because phase detector is a part of it.Any idea about this?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.