STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Phase Detector/comparator

Posted on July 11, 2016 at 16:08Hi,I want to write a phase comparator on my nucleo-f334.As far as I know, it works like this: two signals are sent in the phase detector. When one of them cross the zero line, a timer/counter is started, and it stops ...

antoine by Associate II
  • 1121 Views
  • 0 replies
  • 0 kudos

STM32F0Discovery External Interrupt Configuration

Posted on July 11, 2016 at 09:15Hi, I've been trying to get going with this dev. board, but I ran into problems with the external interrupt. No matter what I choose in     SYSCFG->EXTICR[0], the PA0 interrupt is always the selected one. Can anyone o...

lab by Associate II
  • 2921 Views
  • 5 replies
  • 1 kudos

Cannot change system speed for STM32F746IG

Posted on July 06, 2016 at 09:10I designed a PCB and I am programming the STM32F746IG via a FT2232D chip.  I have the 4 x JTAG signals connected to the STM32.I generate code with MXCube, it compiles, but when I run it, Crossworks goes into an enless...

stm32 uart rx dma broke, is there any idea?

Posted on July 10, 2016 at 11:21I use stm32f427 to do a work,recently, I hope to use dma to get uart rx data,but I found there a strange situation that sometimes the dma will broke and I cannot find whyany other functions keep working, but only the ...

ctc.ctc by Associate II
  • 1351 Views
  • 2 replies
  • 0 kudos

I2C on STM32F1xx.

Posted on July 11, 2016 at 11:59  The original post was too long to process during our migration. Please click on the attachment to read the original post.

stm32f3xx_hal.h

Posted on July 06, 2016 at 14:101. how to set up for fast channel change2 .without recalibration3. how to use SDADC_CONF_INDEX_0 ////////////////////////////////////////////////////////////////////////////////////////// ////////////////////////////C...

nv74 by Associate
  • 1497 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.