2021-05-17 10:49 AM
Hi,
I am trying to interface a PDM mems microphone to my STM32 NUCLEO using some example code I found https://github.com/YetAnotherElectronicsChannel/STM32_PDM_Microphone.
The issue I am having is this code and other things I have read online show the PDM2PCM converting 16 output samples from one call to PDM_Filter().
What I am really trying to do is get a single sample from the microphone when I call PDM_Filter() and send that single sample in a packet (with other information) over UART.
When I change the output sample to 1, do I need to change the number of PDM samples that are received in the PDM_Filter() or in the I2S receive function? I don't seem to be getting good data when I change from 16 output samples to 1.
Any information on this, or a better explanation of the conversion from I2S to PDM to PCM would really be appreciated.
Thanks in advanced.
Some code below.
// Here are the PDM parameters
PDM1_filter_handler.bit_order = PDM_FILTER_BIT_ORDER_MSB;
PDM1_filter_handler.endianness = PDM_FILTER_ENDIANNESS_BE;
PDM1_filter_handler.high_pass_tap = 2104533974;
PDM1_filter_handler.in_ptr_channels = 1;
PDM1_filter_handler.out_ptr_channels = 1;
PDM_Filter_Init(&PDM1_filter_handler);
PDM1_filter_config.decimation_factor = PDM_FILTER_DEC_FACTOR_64;
PDM1_filter_config.output_samples_number = 16;
PDM1_filter_config.mic_gain = 0;
PDM_Filter_setConfig(&PDM1_filter_handler, &PDM1_filter_config);
// Below are my I2S and PDM calls
HAL_I2S_Receive_DMA(&hi2s2, &pdmRxBuf[0],64);
PDM_Filter(&pdmRxBuf[0],&MidBuffer[0], &PDM1_filter_handler);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.