2019-04-07 2:40 PM
I found the doc AN4666 and AN2548, but I could not come to a conclusion.
I have the STM32F103C8T6, but when performing a sequence of 1000 readings, the average time was of 266us, approximately 3.759398 MHz.
I would like to know which chip model should I use to be able to receive data from the external ADC at a frequency of 20 MHz and 8 bits (TLC5510), with external clock, managed by external interrupt (ADC clock)?
Thank you.
2019-04-09 11:13 AM
I also asked on the ADC manufacturer's website if it is safe to overclock this AD9288-40 to get 100MSPS but had no answer yet. Scary!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.