2019-04-07 2:40 PM
I found the doc AN4666 and AN2548, but I could not come to a conclusion.
I have the STM32F103C8T6, but when performing a sequence of 1000 readings, the average time was of 266us, approximately 3.759398 MHz.
I would like to know which chip model should I use to be able to receive data from the external ADC at a frequency of 20 MHz and 8 bits (TLC5510), with external clock, managed by external interrupt (ADC clock)?
Thank you.
2019-04-07 4:05 PM
Wouldn't an FSMC implementation work faster? DCMI has better speed.
Or a FIFO buffer http://www.averlogic.com/AL422B.asp capture at high rates, pull as fast as possible
What do you plan to do with the data?
2019-04-08 9:49 AM
Hi, FIFO is a good idea, I was thinking of using some buffer made with parallel SDRAM, but the FIFO is already done. Thank you!
But, I would like to know how to get 200MSPS from a 40MSPS ADC. Using only one STM32F407VET6 and one adc AD9288BSTZ-40. Look at this analysis of this DSO338:
https://lygte-info.dk/review/Equipment% ... %20UK.html
2019-04-08 10:02 AM
I found something about this in this post, I'll try to find some sample code to test:
2019-04-08 10:33 AM
That's a nice non cheap chip. Could be interesting to have HW FIFO logic with SRAM in STM32?
2019-04-08 10:49 AM
I found the AN5020 (Digital camera interface (DCMI) for STM32 MCUs) but seems that DCMI is only for:
STM32F2x7
STM32F407/417
STM32F427/437
STM32F429/439
STM32F446
STM32F469/479
STM32F7x5
STM32F7x6
STM32F7x7
STM32F7x8
STM32F7x9
STM32L4x6
STM32H7x3
And I found the AN3241 (QVGA TFT-LCD direct driveusing the STM32F10xx FSMC peripheral)
2019-04-08 12:06 PM
They presumably over-clock the part, and interleave the two ADC
https://www.analog.com/media/en/technical-documentation/data-sheets/AD9288.pdf
2019-04-08 4:38 PM
Hummm...
Overclock 40MSPS to 100MSPS?
It does not make much sense for the manufacturer to make a 100MSPS version if the 40MSPS version can reach 100MSPS.
If it was the 100MSPS version, using the interleaved channels, maybe, sounds good.
The best way to check this would be to measure the ADC clock?
I find it interesting, the STM32F407VET6 can generate a clock of 100MHz?
2019-04-08 8:37 PM
And how will you process the incoming data if the data rate is higher than the max SYSCLK?
2019-04-09 11:11 AM
I found this video on the use of interleaved ADCs, it is very interesting what manufacturers may be doing:
What? 5x AD9288-40 (40MSPS) to get 1GSPS???????
[EEVblog #19 - Rigol caught with their pants down!]
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.