2020-02-19 2:18 AM
Dear all,
ST brought a new feature to the STM32H7A/B and some L4+ MCUs, the "parallel synchronous slave interface (PSSI)". We would like to use this for a fast host-to-host communication. But this interface seem so new, we could only find register description in the RM0432 Reference manual. Are there any code example or app-notes for PSSI host-to-host communication?
Thanks.
Solved! Go to Solution.
2020-02-28 3:36 AM
Hi @Michael Schmid ,
To answer your question: I assume this was just the example choice as PSSI can be configured in both 8-bit or 16-bit parallel data input or output.
Then, it may also be related to hardware constraint: we don't have all required pins available in both boards for 16-bit mode.
For my curiosity: could you please explain how will you be using this interface as a host-to-host while PSSI is operating in slave mode? Which device will be connected in your case? For the example, we used 2 NUCLEO-H7A3ZI-Q.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-02-19 8:37 PM
To answer my own question: I have found a great example under
The only question open now for me: In the above example, only 8 bit data width is used. What changes would be required to use a 16 bit wide bus? Is there a reason, why only 8 bit, out of the available 16 bit, was used?
2020-02-28 3:36 AM
Hi @Michael Schmid ,
To answer your question: I assume this was just the example choice as PSSI can be configured in both 8-bit or 16-bit parallel data input or output.
Then, it may also be related to hardware constraint: we don't have all required pins available in both boards for 16-bit mode.
For my curiosity: could you please explain how will you be using this interface as a host-to-host while PSSI is operating in slave mode? Which device will be connected in your case? For the example, we used 2 NUCLEO-H7A3ZI-Q.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-02-29 6:05 PM
Dear Amel,
To answer your question: when I was writing host-to-host, I was thinking about the function of the chip, not the interface mode. Of course, there will be a master and slaves, as in the example with the 2 NUCLEO-H7A3ZI-Q boards.
About the pin constraint: When I use STM32cubeMX, select the NUCLEO-H7A3ZI-Q board, initialize the default periphery, I can select PSSI with 16 bit wide bus. Could you tell me, what pins are missing for a 16 bit wide implementation?
Thanks.
2020-03-02 1:46 AM
About the pin constraint: When I use STM32cubeMX, select the NUCLEO-H7A3ZI-Q board, initialize the default periphery, I can select PSSI with 16 bit wide bus. Could you tell me, what pins are missing for a 16 bit wide implementation?
==> it is just an assumption, as I didn't reviewed deeply the example.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-09 1:52 PM
Dear community,
do you have the example working as you expected? Recently I try it but the master stuck as no one package were received. With polling and generating pulses with a gpio I accomplish to receive data but it required to have two adittional clocks before DE get low and one or two pulses after. Another observation is that after transmitting a package the clock polarity change from FALLING to RISING. is the any errata?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.