2015-11-09 7:23 AM
Hello,
In a Cube project folder, when I click *.uvprojx, the project opens in Keil toolchain ; I build (0 error, 0 warning, great!!), and ready to run. Likewise when I click *.eww and IAR toolchain.What do I
click to open the project in AC6 ?
2015-11-09 8:32 AM
Hi deschamps.manuel.001,
Yes, SW4STM32 is unlike Keil & IAR. To open an existing project with SW4STM32 you should follow this steps below:• File >>Import• Existing Projects into workspace (>>Next)• Click on “Browseâ€� for the root directory• The projects list is refreshed (select then your project) • Ensure the option Copy projects into workspace is unchecked• Then click Finish.-Syrine –We’re moving the ST Community to a new platform to give you a better and more reliable community experience.