F334 HRTIM missing defines stmf30x.h
Posted on November 09, 2015 at 23:48Concerns stm32f30x.h file and devices who uses it.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on November 09, 2015 at 23:48Concerns stm32f30x.h file and devices who uses it.
Posted on November 06, 2015 at 14:56Hello, i try to start with extSDRAM with open4x9 board stm32f429IG. im Using a CooCox IDE. While i worked with internal SRAM everything was fine. But whe i try to work with external SDRAM(IS42SI6400) 64Mb, i meet ...
Posted on November 09, 2015 at 19:09I am designing a breakout (stamp) board for this controller and I am a bit confused about the hardware configuration of the USB OTG section. Can the VUSB be 5 V, the standard voltage from any USB source? If I want...
Posted on November 04, 2015 at 23:08I'm using the Keil v4 IDE/ToolchainIDE-Version:�Vision V4.70.0.0Tool Version Numbers:Toolchain: MDK-ARM Professional Version: 4.70.0.0The STM32F407VET6 is my full version. So I have 512MB flash.My image s...
Posted on August 20, 2015 at 09:19 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on November 08, 2015 at 22:53Hi, I am running a function that seems to be moving the default vector table, that has been set up for FreeRTOS. After running these 2 functions, USB_MSC_HOST_Init(), and then MSCHOST_DeInit(), I run SystemInit()...
Posted on November 09, 2015 at 16:23Hello, In a Cube project folder, when I click *.uvprojx, the project opens in Keil toolchain ; I build (0 error, 0 warning, great!!), and ready to run. Likewise when I click *.eww and IAR toolchain.What do I click...
Posted on November 02, 2015 at 04:06Hi, I am very new to ST microcontrollers and wanted to know if someone can help me with a schematic for the STM32F302R8T6. The hardware I am designing is a USB to CANBUS tool but I need to know whats the minimal c...
Posted on November 09, 2015 at 11:00 Hello I try to debug my application using printf I write some code to overwrite fputc. My problem is with the function HAL_UART_Transmit_IT of the HAL module It doesn't succeed to s...
Posted on November 09, 2015 at 02:03Regarding http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00039084.pdf - the user manual for the Discovery kit for STM32F407/417 lines: On page 20, in section 4.11 ''Solder b...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.