2020-07-22 2:23 AM
I have a simple code I'm using I2C and TIM2 timer interrupt at 100us.
Initially I suspected the issue comes from HAL_TIM_PeriodElapsedCallback but the code inside this function is really few instructions.
In the main.c there are two calls of Error_Handler, both in SystemClock_Config but I checked and the issues is not comming from there.
Could you please support and advice how can I indentify where is the call of the Error_Handler?
If required I can share the code.
Thanks
2020-07-22 5:38 AM
Set a breakpoint in Error_Handler. The stack trace will show where it came from.
2020-07-22 6:04 AM
Check the return address (LR) to see where it came from.
This is the other reason to use the Error_Handler(__FILE__, __LINE__); form, lot easier to run to ground, and get an end user to report via email/phone.
Have the HardFault_Handler() output actionable data also.
2020-07-22 10:18 AM
Thanks for helping.
Anyway, I am not sure why this error handler does not have an error id. It just seems strange.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.