2025-04-19 10:52 PM
Dear Sir,
We are using the STM32H747 series microcontroller in one of our custom projects.
Could you please recommend a low-cost on-board debugger suitable for this board? Ideally, the debugger should also be compact in size.
Your assistance on this matter is urgently needed and greatly appreciated.
Kind regards,
Samudralankaiah
2025-04-20 2:38 AM
Hello @Samudra and welcome to the ST Community.
I suggest you to have a look at the Hw debugger and programmer tools for STM32 products and try to find the suitable debugger solution for you. Personally, I recommend one of the ST-Link V3 or V2 families (genuine products).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-20 5:31 AM
Use an ST-Link/V3MINIE and put a standard 14-pin header (Samtec FTSH-107-01-L-DV-K) on your board as the interface.
STLINK-V3MINIE - STLINK-V3 compact in-circuit debugger and programmer for STM32 - STMicroelectronics
2025-04-21 9:26 AM
Is it possible to get the schematics of the STLINK-V3MINI board to check this? Could you please provide them?
2025-04-21 9:42 AM
The user manual shows the connector pinout. The schematics are not published.
2025-04-21 12:11 PM
More importantly, the firmware is not provided.
Perhaps use a Tag-Connect footprint to easily attach an external debug pod.
If you've got a budget to buy IP, perhaps look a Segger J-LINK OB for on-board implementation. Or CMSIS-DAP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.