2022-10-24 12:17 PM
I've got my OctoSPI interface working for NOR reads and writes, but Auto-polling is sending too many bytes. The Data Length Register (DLR) is set to 0, for one byte of data, but I get the instruction plus two bytes. If I set the DLR to 1, I get three bytes of data.
Configuration snapshot prior to transaction:
5200:5000 20C0:0001 0000:0000 0018:0800 0000:00C7 ..@ ........G...
CR(0x0): FMODE 2 ( Auto Polling Status mode ) + PMM + APMS + EN
SR(0x0):
5200:5040 0000:0000 0000:0000 0000:0000 0000:0000
DLR(0x40) = 0
CCR(0x100) = 1000001 ( 8 bit IR, single lane, single lane DR)
2022-11-28 4:40 AM
Hello @Community member,
Can you please specify the board/MCU you are using?
Thank you.
Regards,
Chahinez.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.