2026-01-20 3:25 AM - last edited on 2026-01-21 2:37 AM by mƎALLEm
Hi,
Currently I working with Nucleo-H7S3L8 board and trying get XSPI interface up by trying to read memory device ID in STR OPI mode. It is not working yet.
Can someone share detailed steps to get it to working stage? I am able to read id in single SPI mode.
Thanks,
Samiksha
2026-01-21 1:55 AM
Hello,
you'll probably need to send a command to the memory to switch in OPI mode before sending the OPI ReadID command. Please check the memory documentation.
2026-01-21 2:34 AM
Hi,
Could you please point me to the specific command to put memory in OPI mode. I am not able to find one.
I tried to configure RDCR2 for STR OPI mode. Are you talking about any different command?
Thanks,
Samiksha
2026-01-21 2:46 AM
Hello,
>> Are you talking about any different command?
Not sure, because you don't specify the memory you're using.
Please check the guide for maximizing your chances to get an answer from the community:
How to write your question to maximize your chances to find a solution
2026-01-21 2:49 AM
Hi,
I am using MX25UW25645G memory which is already available on Nucleo board.
Let me know if you need any more details.
Thanks,
Samiksha
2026-01-21 6:00 AM - edited 2026-01-21 6:01 AM
There is a sample program to use this memory:
Please check the firmware package for H7RS family which is available here:
Under the folder:
STM32Cube_FW_H7RS_V1.3.0\Projects\NUCLEO-H7S3L8\Examples\XSPI\XSPI_NOR_ReadWhileWrite_DTR
or on github there:
But I don't think it performs an OPI readID.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.