2020-05-05 5:00 PM
I currently have a project using micropython on the Nucleo F401RE. When connected to the virtual USART over usb, it seems to crash every 15min or so. I've tried connecting directly to PA2 and PA3 (while doing all the other setup to enable it) and it runs completely fine without crashing at all.
2020-05-05 5:13 PM
Dell? Disable Diagnostic Agent and Intel Tools
Got most current firmware on ST-LINK?
2020-05-05 6:31 PM
I am on a Dell, but I dont have the Diagnostic Agent nor the Intel tools (as far as i know, after looking through the system).
I've got the most current version of the ST-LINK also (V2.J34.M25), and i've done an update anyway to see if that fixes the problem, all to no avail.
2020-05-05 6:44 PM
Check registry for UpperFilters and LowerFilters
2020-05-05 6:53 PM
Not there unfortunately, here's what i see when i open up the specific GUID class:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.