2020-09-08 10:12 AM
Hi guys
So I am developing a small PWM generator around the F334R8, it's overall extremely simple. All the work is done with another MCU sending data on SPI.
On the F334R8, an EXT interrupt is called when the CS line is pulled down. From there the F3 listens on its MOSI line, grabs the data, and then outputs the 3 PWM channels on its HRTIM1.
That part is working really well.
I wanted to have a failsafe timeout using TIM2 on a 1second timer.
Basically every 1s a timer interrupt is called, and the program checks for a flag. If the flag is down, then I know that it's been 1s without proper data coming in and that the PWM output should be disabled.
For some reason I can't get that simple TIM2 to work.
So I decided to pull the Nucleo board again and create a super simple project that does nothing but toggle a LED on a 1s TIM2 timer.
So I am leaving the custom board issue aside for now, and I would really try to find out what's going on.
the 2 projects are identical, and couldn't be more simple. Your typical Timer Interrupt tutorial you find online.
However, one works and one does not. I wonder if CubeIDE somehow generated code when I had the wrong RCC config and fails to update that on subsequent code generations? I really don't know and that's why I'm here.
I uploaded both of these 2 basic projects here: https://gofile.io/d/1LTvVN
test-timer is the one that is blinking at the wrong frequency
test-timer-2 is the working test, which toggles the LED correctly
both of them are very similar. I went as far as reading the main.c line by line and couldn't find anything obvious. I also generated the pdf report but they didn't help.
I would appreciate if anyone could help steer me in the right direction.
thank you
2020-09-08 1:08 PM
sure enough, it's a different issue on the actual project/board.
the 7,199,999 is correct in it.
the symptoms on it (while in debug, with a break point on the gpio toggle), it triggers once immediately, and then nothing, sometimes it will interrupt again a couple minutes later; sometimes not. I've added that project in case you wish to take a look.
Thanks for helping on this on, I never thought of checking the code automatically generated.
2020-09-08 2:36 PM
My guess is the system is starved of resources. Disable your other callback and/or put a PWM output on a timer channel if you want to monitor it.
You don't mention how often HAL_GPIO_EXTI_Callback is called. Flip an output pin while it's in that interrupt so you have a sense of how long it spends there.
2020-09-08 2:47 PM
The timer interrupt not firing is actually taking place all the time even when I am not sending data over SPI.
Just as a sanity check, in debug I set a breakpoint in both the timer interrupt callback and the EXT gpio callback.
and as expected without sending data, the EXT GPIO callback is not firing. As soon as I start sending data, the EXT GPIO callback fires. That part is working well.
Only that TIM2 interrupt not firing more than once.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.