2015-02-24 7:05 AM
Is it possible to configure external interrupt for blue user button on Nucleo bord (which is PC13) using HAL library?
As given in examples for EXTI_Line0 connected to PA.00 pin: GPIO_InitTypeDef GPIO_InitStructure; __HAL_RCC_GPIOA_CLK_ENABLE(); GPIO_InitStructure.Mode = GPIO_MODE_IT_RISING; GPIO_InitStructure.Pull = GPIO_NOPULL; GPIO_InitStructure.Pin = GPIO_PIN_0; HAL_GPIO_Init(GPIOA, &GPIO_InitStructure); HAL_NVIC_SetPriority(EXTI0_IRQn, 2, 0); HAL_NVIC_EnableIRQ(EXTI0_IRQn);Theoretically for PC13 it should look like: GPIO_InitTypeDef GPIO_InitStructure; __HAL_RCC_GPIOC_CLK_ENABLE(); GPIO_InitStructure.Mode = GPIO_MODE_IT_RISING; GPIO_InitStructure.Pull = GPIO_NOPULL; GPIO_InitStructure.Pin = GPIO_PIN_13; HAL_GPIO_Init(GPIOC, &GPIO_InitStructure); HAL_NVIC_SetPriority(EXTI13_IRQn, 2, 0); HAL_NVIC_EnableIRQ(EXTI13_IRQn);But EXTI13 doesn't exist in HAL library. Any solution?2015-02-24 7:15 AM
> But EXTI13 doesn't exist in HAL library. Any solution?
> Yes: read the manual. [STM32Cube]\Repository\STM32Cube_FW_F4_V1.4.0\Drivers\BSP\STM32F4xx-Nucleo\stm32f4xx_nucleo.h : /** * @brief Key push-button */ #define KEY_BUTTON_PIN GPIO_PIN_13 #define KEY_BUTTON_GPIO_PORT GPIOC #define KEY_BUTTON_GPIO_CLK_ENABLE() __GPIOC_CLK_ENABLE() #define KEY_BUTTON_GPIO_CLK_DISABLE() __GPIOC_CLK_DISABLE() #define KEY_BUTTON_EXTI_IRQn EXTI15_10_IRQn2015-02-24 10:57 AM
Thank you!
2015-02-26 5:29 AM
To help someone a lammer like me, that's how I did it:
void MX_GPIO_Init(void){GPIO_InitTypeDef GPIO_InitStruct; /* GPIO Ports Clock Enable */ __GPIOC_CLK_ENABLE(); __GPIOA_CLK_ENABLE(); /*Configure GPIO pin : PC13 */ GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pin : PA5 */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Speed = GPIO_SPEED_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);HAL_NVIC_SetPriority(EXTI15_10_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);}void EXTI15_10_IRQHandler(void){ if(__HAL_GPIO_EXTI_GET_IT(GPIO_PIN_13) != RESET) { __HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_13); HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5); }}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.