2017-01-18 1:47 AM
I have a system with 1 STM32F407 and 3 STM32F401. The 407 is the master of a communication with SPI with the 3 slaves. On the slave a use SPI in slave mode with DMA in RX/TX. On the slaves the input NSS is used in hardware mode. I have of course three GPIO on master which allow to select one slave after each other. When I try to ask a slave I receive it answer BUT all the three slave answer at the same time. It's like the slave do not take into account the NSS pin.
I have configured the system with STMCube.
I use the HAL library.
/* SPI2 init function */
void MX_SPI2_Init_STEPPER(void){hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_LOW; hspi2.Init.CLKPhase = SPI_PHASE_1EDGE; hspi2.Init.NSS = SPI_NSS_HARD_INPUT; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLED; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED; hspi2.Init.CRCPolynomial = 10; HAL_SPI_Init(&hspi2);}
void MX_DMA_Init_STEPPER(void)
{ /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE();/* DMA interrupt init */
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn); HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);}
HAL_SPI_TransmitReceive_DMA(&SPI_HMI,(uint8_t *)&txAxisBuffer[0],(uint8_t *)&rxAxisBuffer[0],20);
Has someone a solution for me?
Thank you in advance.
#dma-spi-slave-nss-hardware2017-01-18 3:54 AM
Hello
Amez_Droz.Philippe
,For Hardware mode, refer to 'Slave select (NSS) pin management' sectionin the reference manual and check
your configuration according tothe alternate function table andDMAconfiguration.
Also, you can review this discussion
https://community.st.com/0D50X00009XkVu6SAF
,it may helpful for you.STM32CubeF4
v
1.0
firmware packageprovides a full set of SPI examples which canhelp you to identifyyourproblem and confirm if it seems related to the hardware or software environment:STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Examples\SPI
Hope this helps you.
Regards
Imen
2017-01-18 9:46 AM
As an alternative, make nss software, and on each slave, use exti interrupt to activate the processing of the dma transferred data at the rising edge and re-prep the dma for the next transfer. Use exti falling edge to activate MISO pin.
2017-01-18 2:31 PM
Thank you IMEN D for your very fast answer.
Ig I read
https://community.st.com/0D50X00009Xki6JSAR
I understand that there is perhaps a bug in the STMCubeMX 4.13 around NSS.It should be corrected in version 4.14. If someone can saya me what are the modification to do in the soft generated by version 4.13 it would be nice because I modify the fille generated a lot before use them (use of the same software (byte to byte) for different plateform) The link inhttps://community.st.com/0D50X00009Xki6JSAR
is nom more valid.Thank you very much.
2017-01-18 2:32 PM
Thank you KIC842852. It's a good idea, I will use it if it's not possible to have a correct solution without make-up.
Thank you again.
Best regards.
2017-01-19 1:46 AM
Hi
Amez_Droz.Philippe
,I recommend you to use thethe last version of your Cube firmware and CubeMx 4.0 which containsupdates to fix issuesand enhancements implementation as mentioned in the '
'.Hereis the invalid link
https://community.st.com/0D50X00009XkeY6SAJ
.Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.