2016-05-16 4:52 AM
I have a code in STM32f030 whih communicate with an IC through SPI .
My code is SPI_I2S_ITConfig(SPI2,SPI_I2S_IT_RXNE,DISABLE); while(1) { ans_status=notArrived; GPIOB->BRR = GPIO_Pin_12;//select slave delay(40); while(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_TXE)==RESET); SPI_SendData8(SPI2,(u8)(PStartTh+0x80)); while(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_TXE)==RESET); SPI_SendData8(SPI2,(u8)(0xff)); while(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_RXNE)== RESET); t=SPI_ReceiveData8(SPI2); while(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_RXNE)== RESET); t=t+SPI_ReceiveData8(SPI2); while(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_TXE)==RESET); SPI_SendData8(SPI2,(u8)(0xff)); delay(40); GPIOB->BSRR = GPIO_Pin_12;//deselect slave delay(1000); }The device wait for me to send to it 8 bits (the address) , while in this time it does not send anything. After he sends 16 bit data. .While it sends these 16 bit, i send something irelevant (0xff).The point is that NSS stays low ~ 400 usec while SPI Clock cycles run for 1500usecSPI is configured as below: GPIO_InitTypeDef GPIO_InitStructure; SPI_InitTypeDef SPI_InitStructure; GPIO_StructInit(&GPIO_InitStructure); /* SPI pin mappings */ //GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_0);//nss GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_0);//sck GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_0);//miso GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_0);//mosi GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3;//50MHz /* SPI SCK pin configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13; GPIO_Init(GPIOB, &GPIO_InitStructure); /* SPI MOSI pin configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_Init(GPIOB, &GPIO_InitStructure); /* SPI MISO pin configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14; GPIO_Init(GPIOB, &GPIO_InitStructure); /* SPI NSS pin configuration *//* GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &GPIO_InitStructure);*/ /* SPI configuration -------------------------------------------------------*/ SPI_I2S_DeInit(SPI2); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; //SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; /* Initializes the SPI communication */ SPI_Init(SPI2, &SPI_InitStructure); SPI_RxFIFOThresholdConfig(SPI2,SPI_RxFIFOThreshold_HF); SPI_NSSPulseModeCmd(SPI2,DISABLE); SPI_SSOutputCmd(SPI2,DISABLE); SPI_I2S_ITConfig(SPI2,SPI_I2S_IT_RXNE,ENABLE); SPI_Cmd(SPI2,DISABLE); delay(10000);2016-05-16 5:11 AM
You must pair the send/receive as only the send generates clocks, and receive simple reads a register. You must also wait for the receive to complete rather than the TX holding buffer being empty, which occurs about the time the FIRST bit hits the bus, not the LAST.
2016-05-19 4:02 AM
Indeed, just like he said.
this is proper way to read/write to SPI ( you can use dummy read or dummy write if you want only one communication direction, but SPI must be configured for duplex masteruint16_t Read_Write_DAC(uint16_t data)
{
GPIOB->BSRRH=GPIO_Pin_1; //CS low
while(((SPI1->SR & SPI_FLAG_BSY) == SPI_FLAG_BSY));
while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
SPI1->DR=data;
while(((SPI1->SR & SPI_FLAG_RXNE) != SPI_FLAG_RXNE));
GPIOB->BSRRL=GPIO_Pin_1; //CS high
return ((SPI1->DR)>>1);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.