2012-02-19 3:24 PM
The new STM32 MicroXplorer v2.0 is now ready for download, per an automated email that I received from ST. The web page says v1.1, but after downloading, the contents says v2.0 and I verified after I installed it. After you install it, look in the installation directory for the new user manual too. Version 2.0 supports all STM32 devices as of February 2012, except STM32L15xx(C-D) and STM32L162xx. This software is freeware package for Windows to help allocate and configure peripheral mapping to STM32 IC pins.
I updated this information in the wikipedia article too. #microxplorer-stm322012-04-25 5:40 AM
Problem to configure STM32L15x controllers. If I select a pin with the touch controller function all other related pins are also set to TS function and the previous selected function is overwritten. If I try to set a TS pin to one of it's alternate function the hole TS configuration is also relocated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.