STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 MicroXplorer v2.0

Posted on February 20, 2012 at 00:24The new STM32 MicroXplorer v2.0 is now ready for download, per an automated email that I received from ST.  The web page says v1.1, but after downloading, the contents says v2.0 and I verified after I installed it...

sbmeirow by Associate II
  • 1071 Views
  • 1 replies
  • 0 kudos

STM3220G-EVAL ADC noise comes from USB OTG PHY

Posted on April 25, 2012 at 09:01Hello,I have been doing some measurements with the STM3220G eval board using the piece of software at : ./STM32F2xx_StdPeriph_Lib_V1.0.0\Project\STM32F2xx_StdPeriph_Examples\ADC\ADC3_DMAThe ADC reading of the potenti...

EEPROM Emulation

Posted on April 22, 2012 at 00:24The EEPROM emulation demo uses Flash pages 2 and 3 (16 Kbyte pages).  Flash pages 0 and 1 are also 16 Kbyte pages. WHat happens when your program is longer than 32 K?  Is the linker smart enough to skip Flash pages 2...

jihlein by Associate II
  • 2726 Views
  • 7 replies
  • 0 kudos

Problem with USATT, cant receive anything from X-CTU

Posted on April 24, 2012 at 15:57Recently migrate from 8bit MCU to 32bit STM32, I like the FW library, but there is a learning curve required. So I am trying to do a printf with USART, after i compiled the program, i cant receive anything. At this p...

DMA based SPI communication with NSS

Posted on March 06, 2012 at 13:40Hello, while studying the STM32F4xx datasheet i found the following passage:25.3.1: ''The NSS signal is driven low when the master starts the communication and is kept low until the SPI is disabled.''  This leads me ...

mstuehn by Associate
  • 1614 Views
  • 3 replies
  • 0 kudos

STM3210C - Clock Frequency Irregularites

Posted on April 16, 2012 at 22:16Hi all, I am currently using the STM3210C evaluation board and have discovered something which is puzzling, and has to do with the clock frequencies.  I am currently using Atollic to program the board and have initia...

System software reset, effects and privileges

Posted on April 21, 2012 at 16:32Hi all, I'm building a custom bootloader and need to provide a way to write protect/unprotect the memory. In order to commit the change, a system reset is required, which I sought to be a software-triggered reset. Fi...

zavaboss by Associate
  • 2063 Views
  • 3 replies
  • 0 kudos

PWM input capture

Posted on April 23, 2012 at 21:16It looks to me like the hardware for Tim4 will support PWM input capture on channel 3/4,but when I look at the source code for the standard peripheral library  (V3.5.0) the procedureTIM_PWMIConfig appears to be hardw...

Help with application jump to system memory boot

Posted on March 16, 2012 at 13:34Hello, I’m trying to force my device (STM32F417) into system memory boot without physically setting the boot pins (cannot access them) and resetting the board i.e. jump to it from my application when the user reque...

eamonn by Associate II
  • 3385 Views
  • 6 replies
  • 0 kudos

STM32F4-Discovery Audio_playback_and_record Project

Posted on April 23, 2012 at 11:29Hi, I'm trying to test the Audio_playback_and_record Project in the STM32F4-Discovery board, but even if I use the bin file included in the fw package(V1.1.0), the audio quality of the digital mems microphone is very...

spinazze by Associate
  • 802 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.