2021-10-06 2:50 AM
Hello community,
It is possible that an interrupt will be nested over itsef?
I mean, I have one interrupt EXTI0_IRQHandler() and inside the interrupt I am waiting an event that requires the execution of the same interrupt.
I read the PM0214 and it is said that "Preemption When the processor is executing an exception handler, an exception can preempt the exception handler if its priority is higher than the priority of the exception being handled"
In my case, Could I change the prioriry of the IRQ dinamically so the new event will be processed as a new IRQ nested with the same IRQ??
Thank you very much for your help
Solved! Go to Solution.
2021-10-06 6:52 AM
An interrupt cannot preempt itself. It will get fired again after it completes if the relevant flags are still set.
2021-10-06 6:05 AM
Paul
2021-10-06 6:52 AM
An interrupt cannot preempt itself. It will get fired again after it completes if the relevant flags are still set.
2021-10-06 7:58 AM
What do you need to achieve in the hw ?
2021-10-07 12:53 AM
I think as TDK said that it is not possible to have the same interrupt nested inside itself.
I did a workaround to solve the situation.
Thank you all for your answers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.