2018-01-18 1:23 AM
Hello, I'am using STM32F746IG and I have a problem with writing data to the Nand Flash memory via the FSMC . When I generate a project with CubeMx, configuring only the flash memory, everything works, i.e. writing, reading, erasing, reading ID etc. The problem starts when I add TIMER to the project (or anything that generates an interrupt), then in the pages appears mistakes. Could this look like a connection to the __DSB barrier? What happens when __DSB is executing and the interrupt call?
#interrput #fsmc #nand-flash #__dsbWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.