2018-01-18 12:42 AM
Is it possible to map timer trigger output signal to a GPIO pin. Typical use-case for my application is to trigger an external adc with the same signal which is used to trigger internal ADC on MCU. The MCU in question is F303.
2018-01-18 1:22 AM
Not directly. You can feed it as TRGI to other timer (if there's such link and the slave timer is available), and use it to trigger a one-pulse process which some of the outputs set to PWM. There will be some latency.
It may be much simpler to use those ADC triggers which are sourced in TIMx_CCy, e.g. regular EXT0 (EXTSEL = 0) triggers from TIM1_CC1 event event.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.