2017-09-26 8:09 PM
Hi, I have a small custom board using an STM32L0xxx.
The RTC is running as expected in run mode.
When I enter Standby mode the RTC appears to stop.
The MCU is in standby most of the time, it wakes up for about 2 to 4 ms, checks some digital and analogs and goes back to standby for about 600ms.
What I am seeing is the RTC time freeze during standby, the RTC is working in run and the MCU wakes up OK.
Currently I am using the LSI oscillator for the RTC.
Im not sure whether I have an issue with the RTC or with the Standyby config??
Here is my code entering Standby:
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
HAL_RTCEx_DeactivateWakeUpTimer(&__g_rtc);
HAL_RTCEx_SetWakeUpTimer_IT(&__g_rtc, sleepTime, RTC_WAKEUPCLOCK_RTCCLK_DIV16); //0x0610 /* Clear all related wakeup flags */ __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); HAL_PWR_EnterSTANDBYMode();Here is the clock Init: sorry its a bit ugle looking, all of this is called with each wake up.
void sys_clock_init(int funct) // funct 0 = full init, 1 = ??
{ RCC_ClkInitTypeDef clk; RCC_OscInitTypeDef osc; __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);// Enable HSI Oscillator and activate PLL with HSI as source.
osc.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI; osc.HSEState = RCC_HSE_OFF; osc.HSIState = RCC_HSI_ON; osc.LSIState = RCC_LSI_ON; osc.PLL.PLLState = RCC_PLL_ON; osc.PLL.PLLSource = RCC_PLLSOURCE_HSI; osc.PLL.PLLMUL = RCC_PLLMUL_4; osc.PLL.PLLDIV = RCC_PLLDIV_2; osc.HSICalibrationValue = 0x10;if (HAL_RCC_OscConfig(&osc) != HAL_OK) {
sys_error(); }// Select PLL as system clock source and configure dividers.
clk.ClockType = RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2; clk.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; clk.AHBCLKDivider = RCC_SYSCLK_DIV1; clk.APB1CLKDivider = RCC_HCLK_DIV1; clk.APB2CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&clk, FLASH_LATENCY_1) != HAL_OK) {
sys_error(); }// Required for HAL_Delay to work correctly
__HAL_RCC_TIM2_CLK_ENABLE(); __TIM2_CLK_ENABLE();// move stuff here that is not required in init after sleep
if (funct == 0) {}
}
// Initialize low power management.void sys_lp_init(void){}// Initialize the LSE clock which is used by LPUART.
void sys_clock_lse_init(void){ RCC_OscInitTypeDef osc;osc.OscillatorType = RCC_OSCILLATORTYPE_LSE;
osc.PLL.PLLState = RCC_PLL_NONE; osc.LSEState = RCC_LSE_ON;if (HAL_RCC_OscConfig(&osc) != HAL_OK) {
sys_error(); }}// Initialize the LSI clock which is used by LPTIM and RTC.
void sys_clock_lsi_init(void){ RCC_OscInitTypeDef osc;osc.OscillatorType = RCC_OSCILLATORTYPE_LSI;
osc.PLL.PLLState = RCC_PLL_NONE; osc.LSIState = RCC_LSI_ON; osc.LSEState = RCC_LSI_OFF;if (HAL_RCC_OscConfig(&osc) != HAL_OK) {
sys_error(); }}// Initializes the RTC based on the LSI.
// Notes: The LSI **must** be initialized prior to this.void sys_rtc_init(void){ // Configure LSI as RTC clock source RCC_PeriphCLKInitTypeDef pclk;pclk.PeriphClockSelection = RCC_PERIPHCLK_RTC;
pclk.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;if (HAL_RCCEx_PeriphCLKConfig(&pclk) != HAL_OK) {
sys_error(); }// Enable the RTC clock
__HAL_RCC_RTC_ENABLE();// Enable NVIC for RTC alarm
HAL_NVIC_SetPriority(RTC_IRQn, 0x0, 0); HAL_NVIC_EnableIRQ(RTC_IRQn);}If any one can help that would be great.
Thanks
Kevin
2018-11-05 10:55 PM
Hello, I have the same problem. I'm using STM32F076 and after wakeup from standby, the RTC time is stuck to the time before it entered the standby mode. Why is the RTC time frozen in this case?
2018-11-05 11:55 PM
Probably because the LSI isn't in the low power domain.
2018-11-06 12:33 AM
Hi Clive. According to the Reference Manual, the RTC clock and calendar still runs even in Standby mode given that LSI is used.
From the Manual:
"The RTC remains active when the RTC clock source is LSE or LSI. RTC alarm, RTC
tamper event, RTC timestamp event, and RTC Wakeup cause the device to exit the
Standby mode."
In my understanding, the RTC should still continue running, and it was able to alarmon the designated time so it should be running. Is my understanding correct?
2018-11-06 2:08 AM
From RM0377:
In Standby mode, the following features can be selected by programming individual controlbits:
...
Are you sure both bits are set and the RTC is configured?
2018-11-07 2:26 AM
Hello, don't mind this question. Actually, the RTC time isn't freezing after standby. I was printing the "Set alarm time" and then "wake up time" and wondered why they are equal. Of course, they will be equal because the wake up time (after standby) should be equal to the alarm set.
2020-08-13 10:52 PM
This happens when you have a wake time below 1 second. Just like the second is always written to the same value. The dirty solution was to count the number of wakes and adjust the rtc. Not accurate its off 10 munites a day.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.