2018-07-03 8:03 AM
I cannot communicate my mpu6050 with nucleo-F103RB board via I2C interface. Here is my code, maybe someone could explain me what is wrong.
&sharpinclude 'stm32f1xx.h'
I2C_HandleTypeDef hi2c;
UART_HandleTypeDef uart;void send_char(char c)
{ HAL_UART_Transmit(&uart, (uint8_t*)&c, 1, 1000);}int __io_putchar(int ch)
{ if (ch == '\n') send_char('\r'); send_char(ch); return ch;}int main(void)
{ uint8_t who_i_am=1;SystemCoreClock = 8000000;
HAL_Init();__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_USART2_CLK_ENABLE(); __HAL_RCC_I2C1_CLK_ENABLE();GPIO_InitTypeDef gpio;
gpio.Mode = GPIO_MODE_AF_OD; gpio.Pin = GPIO_PIN_6 | GPIO_PIN_7; // SCL, SDA gpio.Pull = GPIO_PULLUP; gpio.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOB, &gpio);gpio.Mode = GPIO_MODE_AF_PP;
gpio.Pin = GPIO_PIN_2; gpio.Pull = GPIO_NOPULL; gpio.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &gpio);gpio.Mode = GPIO_MODE_AF_INPUT;
gpio.Pin = GPIO_PIN_3; HAL_GPIO_Init(GPIOA, &gpio);hi2c.Instance = I2C1;
hi2c.Init.ClockSpeed = 100000; hi2c.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c.Init.OwnAddress1 = 0xff; hi2c.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c.Init.OwnAddress2 = 0xff; hi2c.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; HAL_I2C_Init(&hi2c);uart.Instance = USART2;
uart.Init.BaudRate = 9600; uart.Init.WordLength = UART_WORDLENGTH_8B; uart.Init.Parity = UART_PARITY_NONE; uart.Init.StopBits = UART_STOPBITS_1; uart.Init.HwFlowCtl = UART_HWCONTROL_NONE; uart.Init.OverSampling = UART_OVERSAMPLING_16; uart.Init.Mode = UART_MODE_TX_RX; HAL_UART_Init(&uart); HAL_I2C_Mem_Read(&hi2c, 0x68, 0x75, 1, (uint8_t*)&who_i_am, sizeof(who_i_am), 1000); printf('who i am = %d\n',who_i_am); while (1) { }}#stm32l-i2c #i2c-isues #nucleo-f103rb #i2c-issue #stm32f103-halSolved! Go to Solution.
2018-07-03 8:49 AM
It seems you are using the 7-bit address. Try with 0xd0 instead of 0x68.
2018-07-03 8:49 AM
It seems you are using the 7-bit address. Try with 0xd0 instead of 0x68.
2018-07-03 11:11 AM
Thank you man, I coudn't figure out for 2 days what was the problem.
:)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.