2017-05-25 10:07 PM
Hello,
I am developing one application with high speed inputs and outputs.Peripheral requirement for application are as below:1. 4 PWM output with resolution 32bit and 2MHZ clock OR external clock source for PWM with 32bit resolution2. 8 external interrupt pins. Dedicated interrupt request for each interrupt3. One UART(for programming)4. One I2C (100kHz)5. Clock source : external crystal support, clock should be higher than 40MHz.6. Pin count : 32 to 487. Flash : 32kB to 128kBIs any microcontroller available with these features?
Solved! Go to Solution.
2017-05-26 6:21 AM
Hello
Kumbhar.Mukund
,There is a large selection of STM32 microcontrollers which may answer your request.
I recommend you to use the 'MCU Finder' tool (
, or the one embedded in ) to fine tune your choice and the select the suitable one(s).-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-26 6:21 AM
Hello
Kumbhar.Mukund
,There is a large selection of STM32 microcontrollers which may answer your request.
I recommend you to use the 'MCU Finder' tool (
, or the one embedded in ) to fine tune your choice and the select the suitable one(s).-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-26 12:55 PM
Most of the parts only support external crystals to 25-26 MHz, but will take an oscillator source of 50 MHz, check fHSEmax in the Data Sheet.
The EXTI pin interrupts frequently go to a single dispatch point, but the source can be identified and vectored quickly.
Four 32-bit PWM sharing a common clock/period is achievable in a number of parts, and rates well north of 2 MHz.
F401?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.