2014-05-13 12:45 PM
I am facing a strange problem using STM3205RBT6
Sometimes when I power up my controller it does not get start executing the code.First line of my code is to configure a pin output & toggle it. Sometimes it doesn't happen.Most of time code works fine. When code does not run, then on connecting external debugger code starts running.I was looking to attach my circuit in pdf format, but I found no such link here. Circuit is simple connecting all capacitors according to datasheet except on reset a 10K pull up & 0.1uF decoupling cap is connected.I had also monitored the reset pin via oscilloscope no noise on it which could make it reset. Update (Guess) : I am using keil. It has function system_init() before entering main(). Possibly PLL get stuck sometimes & not get started. I have to add some counter which can break while loops in it. I am using PLL to create 120Mhz.System_init file is created using excel utility provided by STDo anyone have same problem.How to solve this problem.2014-05-13 12:58 PM
Or if the HSE doesn't start, and you attempt to use that as a source for the PLL.
I guess you need to recognize when the HSE and/or PLL don't start, and have some fail-over option using the HSI (which should start), and use a GPIO or USART configured real early to provide some diagnostic output.2014-05-22 10:00 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.