2017-06-22 12:37 AM
Hello all,
I am using two different timers(TIM2 and TIM3) in order two measure frequency and duty cycle of two independent signals.
As the example guides, i used the HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) function to make those measurements, but I succeeded to get a measurement only for one signal.
What I have to change/add to this function in order to make those two measurements in the same time.
Thanks.
Here is the full function:
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{ if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_2) { /* Get the Input Capture value */ uwIC2Value = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2);if (uwIC2Value != 0)
{ /* Duty cycle computation */ uwDutyCycle = ((HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1)) * 100) / uwIC2Value;/* uwFrequency computation
TIM1 counter clock = (RCC_Clocks.HCLK_Frequency) */ uwFrequency = (HAL_RCC_GetHCLKFreq()/2) / uwIC2Value; } else { uwDutyCycle = 0; uwFrequency = 0; } }}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.