2023-08-29 3:08 AM
I am measuring temperature from sensor via i2c in a loop with one second delay. There are various other functions also in loop. Those functions may take time from 10ms to 500 ms depending on Rx_Callback.
I need to measure rate of change of temperature from sensor. I can implement HAL_Gettick() to get accurate time internal between two measurements. But I am afraid that HAL_Gettick() counter will reset to 0 after few days.
Is there any other way to measure accurate timing between two measurements of temperature ?
2023-08-29 3:26 AM
> But I am afraid that HAL_Gettick() counter will reset to 0 after few days.
So what? Shouldn't be a problem with the correct unsigned integer calculations.
2023-08-29 6:25 AM - edited 2023-08-29 6:26 AM
HAL_Gettick resets after ~50 days.
Temperature rate of change is generally slow. A better method would be measure the change over the past ~minute or 10 seconds or something. 10ms is too quick for this measurement, the resolution of a temperature sensor is quantized and isn't going to yield an accurate delta over such small time scales.
Using HAL_GetTick is fine. Could also use a timer to get more accuracy, but timing accuracy isn't going to help much here.
2023-08-29 9:45 PM
rate = (T2- T1)/(Tick2- Tick1)
when counter is reset, Tick1 : XXXXXX (some big number)
Tick2: 0
At this step, the calculated rate will be wrong. please correct me where I am wrong.
2023-08-29 9:51 PM
yes, I think i didn't write clearly. I am measuring temperature every one second approx. There is while loop with one second delay.
Basically needs temperature gradient to know if there is any fire or abnormal heating.
I was thinking to use one second time for gradient calculations but isn't tick from Hal_Get give me more accurate time between two time measurements.
I also want to avoid using Timer.
2023-08-30 1:30 AM
Check unsigned integer arithmetic, I think it's called wrap-around when an overflow occurs. So make sure that the tick difference is an unsigned value, then it should always give the correct number - if I'm not mistaken...
So do something like this:
uint32_t u32TickNow = HAL_GetTick();
uint32_t u32TickDiff = u32TickNow - u32TickOld;
u32TickOld = u32TickNow;
rate = (T2 - T1) / u32TickDiff;
2023-08-30 6:35 AM
For HAL_GetTick, which uses a uint32_t counter, the calculation will be correct. That is why it was chosen that way. Convince yourself:
uint32_t start = 0;
uint32_t end = 0;
start -= 42;
// verify that start is a large value and end == 0
uint32_t delta = end - start;
// verify that delta == 42
2023-08-30 2:23 PM - edited 2023-08-30 2:24 PM
The next C standard, C23, will (or already does) support sized integer types other than 8/16/32/64 bits. This compiler will correctly handle the same unsigned wrap-around trick with, for example, 24-bit values.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.