2013-04-09 11:33 PM
I am a new bird for this MCU. My project has two part:
(1) Main program: Using the ST MCU (P/N: STM32F100C8) totransfer data in and out
witha Bluetooth-module through USART interface and then to Android phone:
ST MCU <--> BT module <--> Android, (all communicate with each other by USART interface)(2) Firmware update: I would like to do the firmware update function to update the main program byan Android phone which sending the update firmware to ST MCU throughBT-module by also USART interface.
I spent quite a lot of time searching method in this forum and other websites,
But I just cannot make sure some method like bootloader or DFU is the way I should keep going. I have also checked many application note e.g. AN2606, AN3155 and AN3374... but seems that I do not have enough information to figure out the picture.2013-04-10 3:18 AM
Please try to keep a single thread for this.
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/MCU%20firmware%20update%20with%20USART%20interface%20for%20STM32F100C8&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=1]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fMCU%20firmware%20update%20with%20USART%20interface%20for%20STM32F100C8&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FAllItems.aspx¤tviews=1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.