2017-06-22 3:43 PM
Posted on June 23, 2017 at 00:43
Hello,
I am having more or less the same kind of problems than the one in this post
<LINK NO LONGER ACTIVE>
I am trying a very simple program: a read IO block directly connected to a IO Write block. I started with Matlab R2015b, and after getting lots of errors I installed Matlab R2017a and now I am getting a different kind of errors, in particular this one: Attempt to call a non-function value: SLibModelInitFcnName
More details:
uVision 5.23
STM32CubeMx 4.21
STM32-MAT/TARGET 4.4.1
IOC file generated using the STM32F334 Nucleo discovery board setup, this is also the board that I have.
¿Is this really a problem related to my Matlab's version?¿Does a workaround exist?
I find this whole setup process very absurd and time consuming. ¿Does this really pay off when is up and running?
Here is the whole diagnostics prompt:
The 'ARM CMSIS SIN COS' code replacement library includes the standard math library 'C89/C90 (ANSI)'. To avoid this warning, you can specify the code replacement library as 'None' or remove the base CRL specification if applicable, then select the desired math library via the standard math library (TargetLangStandard) parameter. [2 similar]
### Real-Time Workshop build procedure for method: 'entry
### modelName: 'untitled
### gcs: 'untitled
### bdroot: 'untitled
### Starting Real-Time Workshop build procedure for model: untitled
### Windows version:win64
### Model connectivity is: normal
### Create verification block: None
Code Generation 2 1
Elapsed: 7 sec
### Generating code into build folder: C:\Users\Enrique\Desktop\Test\untitled_stm32
Source 'untitled/GPIO_Read' specifies that its sample time (-1) is back-inherited. You should explicitly specify the sample time of sources. You can disable this diagnostic by setting the 'Source block specifies -1 sample time' diagnostic to 'none' in the Sample Time group on the Diagnostics pane of the Configuration Parameters dialog box.
Component:Simulink | Category:Block warning
----------->STM32 MCU:stm32f3
### Real-Time Workshop build procedure for method: 'before_tlc
### modelName: 'untitled
### gcs: 'untitled
### bdroot: 'untitled
### before_tlc
### Invoking Target Language Compiler on untitled.rtw
### Using System Target File: C:\MATLAB\STM32-MAT\STM32\rtw\stm32.tlc
### Loading TLC function libraries
### Initial pass through model to cache user defined code
Warning: '---------->STM32_Config: MCU_Name is stm32f3'
.
### Caching model source code
Warning: simMode value is 0.0 0:RTW 1:PIL 2:EXT
Warning: Create real-time application main.c
Error: File: C:\Users\Enrique\Desktop\
Test
\untitled_stm32\tlc\customRoutineProcess.tlc Line: 359 Column: 27
Attempt to call a non-function value: SLibModelInitFcnName
Main program:
==> [00] C:\Users\Enrique\Desktop\
Test
\untitled_stm32\tlc\customRoutineProcess.tlc:<NONE>(359)
[01] C:\MATLAB\R2017a\rtw\c\tlc\mw\formatwide.tlc:<NONE>(483)
Error: File: C:\Users\Enrique\Desktop\
Test
\untitled_stm32\tlc\customRoutineProcess.tlc Line: 359 Column: 47
Values of NULL type cannot be expanded
Main program:
==> [00] C:\Users\Enrique\Desktop\
Test
\untitled_stm32\tlc\customRoutineProcess.tlc:<NONE>(359)
[01] C:\MATLAB\R2017a\rtw\c\tlc\mw\formatwide.tlc:<NONE>(483)
### Writing header file untitled.h
.
### Writing source file untitled.c
### Writing header file STM32_Config.h
### Writing header file untitled_types.h
### Writing header file rtwtypes.h
### Writing header file untitled_private.h
### Writing source file main.c
.
### TLC code generation complete.
### Real-Time Workshop build procedure for method: 'error
### modelName: 'untitled
### gcs: 'untitled
### bdroot: 'untitled
### Real-Time Workshop build procedure for model: 'untitled' aborted due to an error.
Error: Errors occurred - aborting
Solved! Go to Solution.
2017-06-23 4:43 AM
Hello,
please replace STM32/script/customRoutineProcess.tlc
with attached file.
BR
Pascal
________________ Attachments : customRoutineProcess.tlc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyX1&d=%2Fa%2F0X0000000b9u%2FgISxG1oPBjNmXVyZksa0fhzDVJh_tzkWn1HnWL7LOcA&asPdf=false2017-06-23 2:18 AM
Hi
Corpa.Enrique
,I will raised your issue internally to the appropriate team.
Regards
Imen
2017-06-23 4:05 AM
Hello,
this problem is known, and will be fixed in next release.
(I can't attach a file.)
Please replace STM32/script/customRoutineProcess.tlc file
line 179 : %<SLibModelInitFcnName()>(%<SLibModelFcnArgs('Initialize',TLC_TRUE,'')>);
with: %<LibCallModelInitialize()>
and
line 359 :%<SLibModelInitFcnName()>(%<SLibModelFcnArgs('Initialize',TLC_TRUE,'')>);
with: %<LibCallModelInitialize()>
Best regards
Pascal Reynaud
2017-06-23 4:43 AM
Hello,
please replace STM32/script/customRoutineProcess.tlc
with attached file.
BR
Pascal
________________ Attachments : customRoutineProcess.tlc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyX1&d=%2Fa%2F0X0000000b9u%2FgISxG1oPBjNmXVyZksa0fhzDVJh_tzkWn1HnWL7LOcA&asPdf=false2017-08-01 6:41 AM
thank you�
2018-05-16 1:46 AM
This tlc file replacement helped me in Matlab 2018a. Building a subsystem does not work. It gives me an Invalid .ioc file error.
It seems like it doesn't execute the after_tlc procedure.
Any suggestions? Please ask if you need any more information.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.