2015-08-28 6:03 AM
Ok so I have a UDP echo server, the requirement being able to echo UDP packets up to 65499 bytes in size. Test software starts at small packet size increasing the size by one byte , transmitting and expecting the packet to be echoed back.
After some tweaking size of packet echoed is limited to 59192 bytes using a PBUF_POOL_SIZE of 40 and PBUF_POOL_BUFSIZE of 1514. Now if PBUF_POOL_SIZE is increased any more than 40 the test fails early in the sequence at a very small packet size (<256 bytes) - Do not know why, maybe someone can help me understand why this is so???When moving the the PBUF_POOL to external SRAM the packet size is always limited to a maximum of 8872 bytes (1472 x 6) consistently. I can increase PBUF_POOL_SIZE beyond 40 this time but the test always fails at 8872 bytes - Would anyone know why??I thought that maybe the ext SRAM interface was not right so I verified its operation with some test code.Thanks EmilioWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.