STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem Failed firmware Nucleo F411RE

Posted on August 20, 2015 at 11:25Hi.On board I found this file: FAIL.TXT - ''The interface firmware FAILED to reset/halt the target MCU''. The leds LD1 and LD3 of COM remain red. I tried to update firmware with http://www.st.com/web/en/catalog/tool...

LWIP Stack UDP Large Packet Size External SRAM Problem

Posted on August 28, 2015 at 15:03Ok so I have a UDP echo server, the requirement being able to echo UDP packets up to 65499 bytes in size.  Test software starts at small packet size increasing the size by one byte , transmitting and expecting the p...

I2C2 Busy flag after clock enable

Posted on August 25, 2015 at 16:53I know it's a recurring problem. I could'nt make I2C2 work on my STM32F401VET.When I use RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE);I2C2->SR2 =2No matter what I do.I try many work around proposed on this fo...

germain by Associate II
  • 3505 Views
  • 9 replies
  • 0 kudos

Program stuck in startup_stm32f4xx.s

Posted on August 28, 2015 at 10:58I am trying to run an existing code developed in Eclipse + GCC in IAR workbench. After making all the related changes, the code compiles successfully. Now when I try to run the program, at the point where there is a...

sommer by Associate II
  • 1647 Views
  • 2 replies
  • 0 kudos

HAL I2C slave with read/write

Posted on August 27, 2015 at 13:08Hi,I've been looking over an example of master/slave I2C communication using an interrupt and I just can't seem to figure out how it actually works. The description is really vague and the HAL documentation isn't mu...

STM32L051: clear PWM output on COMP2 trigger.

Posted on August 26, 2015 at 17:32 I am quite new to STM32 and try to do my second application using an STM32L051K8T6 where I need a PWM signal that is aborted when current rises above a treshold. It didn't take me too long to get this working o...

bart2 by Associate II
  • 3931 Views
  • 8 replies
  • 0 kudos

DCMI + DMA - empty buffer

Posted on August 28, 2015 at 09:05Sorry for my bad English, I use a translatorMCU: STM32F429I use CoCoox. I wrote code to initialize the camera. Interrupts DMA2_Stream1_IRQHandler and DCMI_IRQHandler triggered, but the buffer is empty when I want to...

Stm32l052 temperature sensor calibration problem

Posted on August 21, 2015 at 17:49Hi. I am working on the temperature controller using stm32l052. I use inbuilt temperature sensor. What am I doing wrong? TEMP130_CAL_ADDR value here is 0x0395 = 917dec TEMP30_CAL_ADDR value here is 0x029d = 669dec T...

baev_al by Associate III
  • 1314 Views
  • 4 replies
  • 0 kudos

Read back RAM contents on STM32F302R8

Posted on August 27, 2015 at 02:02Hi, I am running a small program on my nucleo board and it would be very helpful to read back the RAM contents during processing. The IRAM is set in Keil to start @ 0x20000000. But if I set a breakpoint in my code a...

karthik2 by Associate II
  • 2271 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.