2017-07-06 7:46 PM
Hi There,
I am using STM32F429ZI discovery board to write an UART and
LTDC code.
I have Entesla serial to USB converter connected to the Discovery board via TTL(I am not using RS232).
Simple use case is -Display the characters entered from PC hyperterminal.
Now Individually the USART and LTDC code are working from the following git repository, but when I merge them both only USART is working. I can see only flickering on display when I am entering characters.
I am attaching the main file here.
I am using library/code from here -
https://github.com/MaJerle/stm32f429
Any suggestion guidance is welcome.
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.