STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

more uart ports

Posted on July 06, 2017 at 21:02Hi,My stm32 board has four uart ports. Each of them is connected to rs 485 transmitter (tx only).I'm looking for any ideas how to extend my project to have more than four uart ports - up to 10.My first idea was to con...

John Doe1 by Associate III
  • 2469 Views
  • 5 replies
  • 0 kudos

printf swo on stm32l0x1 m0+

Posted on July 06, 2017 at 15:00Designing own board based on stm32L0x1 and looking at debug provision.Am I right in thinking that printf style output is not available via the debugger ( ST-LINK/V2) on the stm32L0 (m0+) parts as:-1) They only have SW...

Stm32User by Associate III
  • 2010 Views
  • 3 replies
  • 0 kudos

possible bug in clock generation

Posted on June 09, 2017 at 09:26I am using cube 4.21 with a STM32F205 CPU.I configured the clock to run at 120 Mhz (25Mhz crystal M=20, N 192, P 2) in the file system_stm32f2xx.c generated by cube, I have the following:uint32_t SystemCoreClock = 160...

Adalgiso by Associate II
  • 1738 Views
  • 3 replies
  • 0 kudos

How to program ''single byte'' to STM32 internal flash?

Posted on July 06, 2017 at 04:17Hi, all!    I want to program single byte to internal flash, but the standard peripheral library only support 'word' and 'half word', is it possible to program single byte, please?For example: mailto:0x11@0x08010000, ...

Resolved! Interrupts - USART corrupted data

Posted on July 04, 2017 at 11:16Hi everyone,I am designing a system that needs a bunch of interrupts working. By now I have three possible source of interrupts working:+ USART6+ SPI2+ TIM6The USART6 works sending and receiving data from PC.When SPI2...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.