2016-08-02 6:02 AM
I'm working on a project with the stm32l432 which really requires a minimalist approach with respect to code. I like cube for pin assignments, and configuration, but it doesn't appear there's a way to generate the init calls to the low level libraries. Am I missing something ? Are there plans to integrate the low level libraries with cube in a more meaningful way ?
;2016-08-02 6:26 AM
> Am I missing something ?
Downloaded the Cube package for M7 recently, and found the LL layer to be but a sorry stub (two meager files). I suspect their software people just can't keep up with demand. And the LL layer would be the only thing I would ever consider to use.
2016-08-03 1:37 AM
Hi brown.geoffrey.001,
The initialization code generated by MX is based on HAL drivers.Thanks for your suggestion! I will forward it to our MX team.-Syrine-2016-11-15 7:20 AM
Please note STM32CubeMX support generating code based on LL drivers for L4 series.
Use the Advanced settings tab from the Project Settings window, to select LL instead of default HAL drivers for code generation.
2016-11-15 3:23 PM
Definitely a step in the right direction. I generated a small project for the stm32l432 nucleo board (but didn't test) that included USB, CRS, and spi.
I had an issue with RCC configuration I couldn't resolve -- CubeMX objected to the default MSI auto calibration, but also wouldn't let me turn that off (??). The generated code was mostly ok. It was necessary to define USE_FULL_LL_DRIVER because the generated code quite needlessly uses the GPIO init structure. This generally leads to bloated code for a very small simplification in coding (but who needs that if the initialization code is generated anyway.Also the gpdsc file had lots of unnecessary HAL sources listed for devices I didn't explicitly configure. This is a problem with previous releases. Since I generate make files from GPDSC, I then have to explicitly disable these files. Why all the bloat ?GeoffreyWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.